제품이 장바구니에 추가됨

What are the advantages of Fiber Optic Illumination?

Fiber optic light guides transmit light based on the principle of total internal reflection. Light incident on cylindrical fibers of either acrylic or glass materials can be transmitted through these fibers with little attenuation.

Useful for applications with very tight space or limited access constraints, Fiber Optic Illumination can provide a wide range of useful illumination geometries from spot lights and ring lights to diffuse sources and line lights. Light guide optics are also able to brave certain environments where using electronics would otherwise be a danger. Fiber optic illumination can also be intensity controlled and very easily aimed towards objects. Broadband illuminator sources provide white light illumination, which is composed of all of the colors of the visible spectrum.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요