Edmund Optics®, a leading global supplier of optical components and solutions, is pleased to announce the addition of Optical Coherence Tomography (OCT) Phantoms and Diffuse Reflectance Phantoms to their extensive product portfolio, now providing off-the-shelf, standardized ready-to-use tools for researchers and engineers for the calibration and optimization of imaging systems in research and clinical applications.
Edmund Optics’ newly added Optical Coherence Tomography (OCT) Phantoms offer a controlled sample for testing and calibrating OCT systems featuring well-characterized optical properties like refractive index, scattering coefficient, and absorption coefficient for ensuring accurate and reliable measurements. Now available off-the-shelf in designs including Point Spread, Multilayer, Pyramid, and Multipurpose, these phantoms ensure accurate testing of system parameters like depth resolution, image contrast, and sensitivity, providing consistency across clinical and research measurements.
Additionally, the newly added Diffuse Reflectance Phantoms simulate the optical properties of biological tissues for calibration, characterization, and analysis in biophotonics applications. Now available off-the-shelf in sizes of 25 x 25 mm and 50 x 50 mm for muscle, brain, and adipose tissue, these phantoms are ideal for applications like spatial frequency domain imaging, diffuse reflectance spectroscopy, diffuse Raman spectroscopy, and more.
The addition of biological tissue phantoms is a significant milestone for Edmund Optics, expanding its portfolio beyond traditional optical components. This step provides off-the-shelf, standardized tools for researchers and industry engineers in biophotonics, while also demonstrating the company’s continued commitment to providing effective, whole-beam-path solutions throughout the customer’s development cycle – from research and development through to volume production.
To view these, and many more exciting new products from Edmund Optics, visit the new products page at www.edmundoptics.com.
About Edmund Optics:
Edmund Optics® is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. The company designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. Operating in more than a dozen major facilities around the globe, Edmund Optics employs just over 1,100 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2023, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)
The FUTURE Depends On Optics®