Lasers can induce photo-thermal and photo-chemical changes to retinal tissue to modify structures responsible for a specific vision impairment, like in LASIK.
Using IR Spectroscopy for Counterfeit Drug Detection
Infrared spectroscopy is used to detect harmful chemicals in counterfeit drugs making it critical to combat the opioid crisis, in the field or the lab.
How Trützschler and ITOS are Creating Cleaner Cotton
How Trützschler utilizes polarization to enable the more efficient processing of cotton providing a cleaner product and reducing rejected material in an effort to reduce waste and be more environmentally friendly.
The future depends on quickly and safely detecting elevated body temperatures that may indicate the presence of contagious diseases, such as COVID-19 (novel coronavirus).
Optics aid in the quick and accurate serological detection of antibodies to determine if a subject has an immune response to COVID-19, or the novel coronavirus.
The future depends on vision-guided technology that can safely sanitize hospitals, warehouses, and other locations to prevent the spread of contagious diseases, like COVID-19 (novel coronavirus).
Laser optics are critical for skin care procedures such as hair removal, acne and scar reduction, tattoo removal, sunspot removal, and skin revitalization.
Researchers from the University of Hawaii at Manoa use telecentric lenses and illuminators from Edmund Optics to advance our understanding of lung function.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2023, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)
The FUTURE Depends On Optics®