제품이 장바구니에 추가됨

Edmund Optics®

지식센터

 검증된 라이브러리로 240명 이상의 글로벌 엔지니어가 참여하여 만든 신뢰할 수 있는 기술 자료를 제공합니다.

필터
Search Results for: Optical Isolators (12)

Semiconductor Supermirrors

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Ruggedized Imaging Lenses

Not all ruggedized imaging lenses feature the same type of ruggedization. Learn about the advantages and disadvantages of each type at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Computer Generated Hologram Metrology

Computer Generated Hologram metrology provides a new solution for overcoming traditional asphere metrology. Learn more about CGH metrology at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Stemmed Mirrors

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

바로 보기 저장된 콘텐츠 목록에 추가

Future of Spherical Lenses

Traditional spherical lenses are evolving due to the increasing demands of applications. Learn about the future of spherical lenses at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Superpolished Optics

Superpolished optics with sub-angstrom surface roughness are ideal for precise laser optics applications

바로 보기 저장된 콘텐츠 목록에 추가

단일 소재의 비구면 아크로매틱 렌즈

Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.

바로 보기 저장된 콘텐츠 목록에 추가

Ultra-Thin Longpass and Shortpass Filters

Innovative ultra-thin filters provide flexibility, scratch resistance, and durability comparable to most hard oxide coatings. Learn more at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Trending in Optics: The Future of Optical Filters

New optical filters are being developed due to the advancements in applications and technologies. Learn more about the future of filters at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Hyperspectral and Multispectral Imaging

Hyperspectral imaging (HSI) and multispectral imaging (MSI) are two related technologies that make use of specialized vision systems to acquire extra image information from extended regions of the electromagnetic spectrum aside from the visible spectrum.

바로 보기 저장된 콘텐츠 목록에 추가

Ultrafast Highly-Dispersive Mirrors

Pulse Compression and Dispersion Compensation for Ultrafast Lasers

바로 보기 저장된 콘텐츠 목록에 추가

Non-Circular Optics for System Miniaturization

Trimming the Fat: Truncating Lenses to Shrink Systems

바로 보기 저장된 콘텐츠 목록에 추가
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요