Design vs. Manufacturing
This is Section 3.6 of the Imaging Resource Guide.
Nominal vs. As-Built
“How will this lens perform?” It may sound like a simple question, but the answer can be complicated. For a machine vision lens, certain factors first must be considered, such as the lighting used, the working distance (WD) to the object, the f/# of the lens, and the sensor size. These are all covered in previous sections. Then the question must be clarified: “how will the lens perform as-built as compared to nominal?
Nominal
Nominal design specifications assume the lens is built exactly as it is designed. By modeling the lens in a ray-tracing design software, such as Code V, Zemax, or otherwise, lens performance for any scenario is predictable and data is easily extractable. This is not always the best answer, though, as it assumes all factors are exactly as specified in the design model and without any tolerances, which is never the case in practice.
As-Built
In contrast, as-built describes the process of using statistical predictions to determine how a lens design will perform with manufacturing tolerances considered. As-built performance is difficult to predict; many factors must be modeled that may alter the performance of the lens, such as absolute position and shape of elements and the index and dispersion of the glass used. A typical tolerance file—the code used to provide the model with all the possible factors—has on the order of 100 to 200 components for a Zemax design simulation and 200 to 400 components for a Code V design simulation; this can vary significantly depending on the number of elements and the ways in which the elements are mounted.
A simplified description for modeling as-built performance is that every parameter is randomly varied, based on the tolerance ranges, and then statistically evaluated to determine how many random assemblies perform adequately. A few parameters are evaluated, such as modulation transfer function (MTF) at specific frequencies and field points; then from this, a probability of the lens reaching the performance requirements can be determined.
A lens’s nominal performance is easily predicted for any configuration and with any criteria, such as MTF, distortion, or spot size by using the prescription information. While this information does not provide as accurate of a prediction as toleranced, as-built performance, it can provide an approximation to the specific circumstances and is a useful comparative tool.
For more tips and information on managing the design of manufacturable lenses and assemblies, read Tips for Designing Manufacturable Lenses and Assemblies.
혹은 지사별 연락처 확인
견적 도구
재고번호 입력 후 바로 시작
Copyright 2023, 에드몬드 옵틱스 코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동 풍성빌딩)