제품이 장바구니에 추가됨

What is the color temperature of a quartz halogen lamp and a metal halide lamp?

The typical color temperature of a typical quartz halogen lamp and bulb such as our 150W EKE Replacement Bulb is 3250 Kelvin, while that of a typical metal halide lamp and bulb such as our 100W Metal Halide Replacement Bulb is 5300 Kelvin. Spectral curves are available by visiting the presentation for each replacement bulb.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program