제품이 장바구니에 추가됨

Is there a limit to the range of angles in which a CGH can be used?

A CGH has a minimum feature size in its interference pattern that limits the maximum possible diffraction angle. This is why an aspheric CGH is often used along with a reference sphere in the interferometer to reduce the required diffraction angles.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program