제품이 장바구니에 추가됨

What is the advantage of high frequency illumination?

High frequency illumination provides a flicker and ripple free output that assures image quality by maintaining constant frame to frame gray level. Fluorescent lights are the best example of high frequency illumination. When determining the correct illumination for one's camera setup, make sure the frequency of the illumination is higher than the frame rate of the camera. This will help to insure constant illumination and therefore the best image quality from frame to frame. Correspondingly, high frequency illumination helps reduce operator fatigue and eye strain when used over long durations.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program