Imaging lenses feature a wide variety of lens mounts, all of which offer different benefits. For a more comprehensive breakdown of these types and what they are useful for, read Lens Mounts. The most common mounts used in machine vision are the C-Mount, S-Mount (M12 mount), F-Mount, TFL-Mount, and TFL II Mount. The C-Mount, S-Mount, TFL-Mount, and TFL II Mount types offer robust stability for machine vision systems whereas the bayonet-style mount of the F-Mount lends itself better to non-industrial, photography-type applications. However, the most useful mount type depends on the size of the machine vision camera sensor being used as well as the optical abilities of the imaging lens.
1-800-363-1992
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2025, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)