제품이 장바구니에 추가됨

Why is it necessary to collimate the laser diode before fiber-coupling?

Strictly speaking, there are optical designs which enable fiber coupling without first collimating the output of the diode laser, but all of these designs suffer from massive astigmatism which can significantly reduce the efficacy of the fiber coupling. Having a collimated beam inside of the laser package allows for the addition of optical elements such as micro-optical isolators and bandpass filters.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program