제품이 장바구니에 추가됨

I’m using the MT-1 Accessory Tube Lens and MT-1/MT-2 C-Mount Adapter. Two thin brass rings came with the adapter. How are they used?

You can use the spacer rings to compensate for little irregularities of the position of the intermediate image plane on the MT-1/MT-2 C-Mount Adapter. They are extremely useful when trying to properly align a setup as the can easily correct for slight misalignment anywhere in the system.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program