제품이 장바구니에 추가됨

I would like to view the side profile of a 140μm diameter glass fiber under a microscope. I am having some difficulty resolving the fiber’s border, is there any special lighting technique to use?

There are multiple ways to achieve the effect you require; however, the most straightforward is utilizing Darkfield Illumination. Darkfield Illumination is ideal for imaging transparent or translucent objects. Light from the Darkfield illuminator, usually a special type of ring light guide, enters the object through the edge, rather than from above, enabling one to see the object’s profile. View Choosing the Correct Illumination for additional information on pros and cons of various illumination setups.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program