제품이 장바구니에 추가됨

What is the difference between refractive and diffractive line generators?

A refractive line generator uses a cylinder or rod lens to focus a laser in only one axis only (drop-moved placement) in order to create a line of light. A diffractive line generator uses a flat optic with an etched microstructure that breaks apart a laser beam and forms an interference pattern in the shape of a laser line. Refractive optics do not correct for the inherent Gaussian profile of a laser beam and form a line with a "hot spot" in the center and fading edges. Diffractive optics will create a line that is uniform in thickness over its length, but is segmented. Diffractive line generators also cause a small portion of the light to be redirected into different diffractive orders, which causes additional faint lines to appear. Some laser line generators use a unique patented Powell glass lens design in order to achieve a continuous (not segmented) line with an even distribution along the length of the line.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program