제품이 장바구니에 추가됨

Will the TECHSPEC Monolithic Reflective Beam Expanders (Mark I) work in reverse (to reduce the size of a beam)?

Fundamentally, these laser beam expanders can work in reverse. However, the specified wavefront values are not guaranteed for reverse operation, and care should be taken to ensure that the input beam diameter is no greater than the specified maximum exit aperture. Also, note that divergence will increase proportionally with the laser beam expander’s magnification.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program