To operate as efficiently as possible, the lenses require the incoming light to be circularly polarized. This requires extra care in the setup, and potentially additional polarization optics in the optical design. Also, the lenses function as a grating, and thus have significant chromatic aberration when used with broadband illumination. Care should be taken to limit the spectral bandwidth of the illumination for optimum results.
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2023, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)
The FUTURE Depends On Optics®