제품이 장바구니에 추가됨

Can wedge prisms be used for beam stearing?

Yes, a pair of wedge prisms can steer a beam anywhere within a circle described by the full angle 4θ, where θ is the deviation from a single prism. This beam steering is accomplished by rotating the two wedge prisms independently of each other, and is typically used to scan a beam to different locations in imaging applications. Two wedge prisms can be used as an anamorphic pair for beam shaping (to correct the elliptical shape of diode outputs).

Beam Steering with Wedge Prisms
본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program