제품이 장바구니에 추가됨

What is the difference between multiple and zero-order retarders and when should I pick one over the other?

Multiple-order retarders (or waveplates) and zero-order retarders are interchangeable. Zero-order waveplates should be considered for more critical applications. The advantages of a zero-order waveplate include an increased bandwidth and a lower sensitivity to temperature changes. A ±2% change from the design wavelength will cause only a minor change in the retardation of a zero-order waveplate. With a multiple-order waveplate, a ±1% change from the designed wavelength will cause considerable problems with the retardation.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program