제품이 장바구니에 추가됨

Do you have C-Mount components to make an in-line illumination assembly?

We offer a C-Mount Light Guide Adapter that will hold a fiber optic light guide on one side by using its corresponding light guide adapter (this stainless steel bushing is not included and is selected based on the light guide's ferrule diameter). The other side has a standard C-Thread for integration with our extensive line of C-Mount components. By using one of our C-mounted Cube Beamsplitters, an in-line system can be assembled. Additional optics can also be inserted prior to the beamsplitter in order to create a collimated light beam from the light guide.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program