To use our #58-877 25mm Cube Beamsplitter Adapter, it is necessary to use the #58-854 TECHSPEC® 1” Diameter Kinematic Mount; the #58-872 TECHSPEC® C-Mount Kinematic Mount, or any other Kinematic mount will not work. This is because the 25mm Beamsplitter Adapter is specifically designed to fit into the 1” Diameter Circular Kinematic Mount where the Nylon-tipped locking screw will secure it into place.
Our line of C-Mount Kinematic Mounts can be integrated with any C-Mount Component; correspondingly, the same applies to our line of T-Mount Kinematic Mounts with any T-Mount Component.
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2023, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)
The FUTURE Depends On Optics®