제품이 장바구니에 추가됨

Do you have any components that would allow me to build a two axis tilt (θ-x, θ-y) platform without any screws protruding up above the surface?

Edmund Optics® offer Metric Goniometers which can be stacked to give two-axis tilt. Our TECHSPEC® Kinematic Table Platforms also have built-in tip/tilt capability. Both of the above the two-axis movement you require without any screws to interfere with your setup.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program