제품이 장바구니에 추가됨

How do I mount a ball bearing linear translation stage to a breadboard table?

The base of each ball bearing stage has 2 counterbored holes that accept socket head cap screws (SHCS). To gain access to the holes, move the mounting stage back and forth. It will help to use the side locking screw to hold the spring in place. The size of the screws depends on the stage; either #4, #6, or ¼. However, the length of the screws depends on the thickness of the adapter plate or the breadboard table (if connecting directly). We currently carry a line of breadboard adapter plates for such requirements with the S.H.C.S. included.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
This site is protected by VikingCloud's Trusted Commerce program