As automated systems expand into a vast array of industries, imaging lenses are being introduced into new environments often experiencing harsh environments. A new generation of ruggedized lenses has been developed to protect from shock and vibration, water exposure, and temperature swings, to enable these automated systems.
This is Episode 9 in the Trending in Optics Video Series, in which one key trend in the optics and photonics industry is highlighted every several months. These conversations seek to shed some light on trending topics in optics and industry. Information on more technological and application advancements can be found at https://www.edmundoptics.com/knowledge-center/trending-in-optics/.
본사 및 지사별 연락처 확인하기
견적 요청 도구
재고 번호 입력 필요
Copyright 2023, 에드몬드옵틱스코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동, 풍성빌딩)
The FUTURE Depends On Optics®