제품이 장바구니에 추가됨
All Press Releases

TECHSPEC® Liquid Lens M12 Imaging Lens Wins Inspect Award at VISION Stuttgart

12/6/2018, Barrington, NJ USA   —

Edmund Optics® (EO), the premier provider of optical and imaging components, is proud to announce that their TECHSPEC® Liquid Lens M12 Imaging Lenses received 2nd place in the Vision category of the 2019 Inspect Awards. The award was presented at the recent VISION Show in Stuttgart, Germany by Anke Grytzka-Weinhold, Editor-in-Chief of Inspect Magazine, and Dr. Heiko Baumgartner, Publishing Director of Wiley-VCH. Winners were voted on by more than 45,000 readers of Inspect, Messtec Drives Automation, and related online communities.

The award recognizes the versatility of the TECHSPEC® Liquid Lens M12 Imaging Lenses, which combine the performance of a compact high-resolution imaging lens with the flexibility of a liquid lens. "The combination of high resolution and integrated liquid lens technology makes the lenses ideally suited for high speed machine vision applications," commented Greg Hollows, Vice President of the Imaging Business Unit for Edmund Optics. "It is an honor to be a recipient of the Inspect Award again and to be recognized for our advanced technology and products."

The TECHSPEC® Liquid Lens M12 Lenses feature a high-resolution f/2.4 optical design with an integrated liquid lens for high throughput with fast electronic focus. This quick autofocus solution uses a two-piece housing design that allows easy access and replacement of the included liquid lens. For convenient access to the liquid lens control cable, the liquid lens can be rotated 180° inside the imaging lens.

TECHSPEC® Liquid Lens M12 Imaging Lenses are part of the M12 offering at Edmund Optics. These compact, high-performance lenses feature precision glass designs in a metal housing, with optimized specifications between each product family. TECHSPEC® Liquid Lens M12 Imaging Lenses are available in four models, with focal lengths at 6.0, 8.0, 12.0, and 16.0mm and working distances from 100mm to infinity through 220mm to infinity. The RoHS compliant lenses feature M12 x 0.5 (S-Mounts). A Liquid Lens Development Kit, which includes a required driver and other accessories, is sold separately. These lenses are in-stock and available for immediate delivery.

About EO:

Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. EO designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. EO’s state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.

 
영업 & 기술 지원
 
혹은 지사별 연락처 확인
사용이 간편한
견적 도구
재고번호 입력 후 바로 시작